Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Where to find the register list for the Easergy P3 relays?
Issue
Where to find the register list for the Easergy P3 relays?

Product Line
Easergy P3 Standard (P3U10, P3U20, P3U30)
Easergy P3 Advanced (P3F30, P3L30, P3M30, P3M32, P3G30, P3G32, P3T32)

Environment
Document

Cause
Need to know what the registers are for the Easergy P3 relay.

Resolution
The only way to see any register and data type map is to use Easergy eSetup Pro in offline or onlinemode. Once you create an Easergy P3 offline configuration file using “eSetup Easergy Pro software” selecting the modbus protocol, then in the communication section you will automatically see the modbus parameters with the register address.

eSetup Easergy Pro: https://www.se.com/ww/en/download/document/eSetup_Easergy_PRO/

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: