{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I change or set digital input assignment in the I/O menu in Somove?
Issue:
Why can't I change the digital input setting in the I/O menu is Somove?

Product Line:
Software

Environment:
Somove

Cause:
In the I/O menu digital input assignments are grayed out. Unable to change.

Resolution:
Digital inputs in the I/O manual are for reading, not writing.
To assign a function to a digital input.
You must go to the function and assign the desired digital input.

Schneider Electric Egypt and North East Africa