1. Issue
In Unity Pro or EcoStruxure Control Expert software, the following popup could be displayed on TSX CPP 110 screen validation after selecting a *.co file of the Sycon tool:
“Cannot load configuration from the database specified!
Error when reading configuration from DBM file. (…)”
2. Product Line
Unity Pro / EcoStruxure Control Expert, Sycon, TSX CPP 110 CANopen PCMCIA card
3. Resolution
The complete name (path + file name) of the *.co file selected in the TSX CPP 110 screen must be less than or equal to 126 characters.
The directory containing the CANopen file must also have read/write access.
Released for:Schneider Electric Egypt and North East Africa