{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the NetShelter AV busbar be installed into other NetShelter cabinets?
Issue:
AR8395 mounts to the accessory rail in the cabinet so it should be able to install into any NetShelter cabinet.

Product Line:
AR8395

Environment:
All versions and serial ranges.

Cause:
AR8395 description says that it's for the NetShelter AV cabinets.

Resolution:

The AR8395 can be installed into any NetShelter cabinet that has 20U vertical mounting space available.

Schneider Electric Egypt and North East Africa