{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the Smart-UPS Self-Test function work?

Article available in these languages: Spanish, Russian


Issue:

Operation of Smart-UPS Self Test

Product Line:

Smart-UPS, Smart-UPS Online

Environment:

All models, All Serial Numbers

Cause:

All Smart-UPS products feature automatic true load self tests.

Resolution:

By default all Smart-UPS products will perform a Self Test when you initially turn the UPS on, and then once every 2 weeks from that point forward. This can be adjusted via PowerChute, the LCD Screen, or the Network Management Card. The interval will always begin when you last turned the UPS on. There is no way to schedule it to run at a particular time or day.

During a Self-Test the UPS will run on battery for approximately 10 seconds. During this time it will test it's internal subsystems as well as the battery. For a battery test to be valid, it should be charged to 100% before beginning the test.  If an issue is encountered the self test will be aborted and the UPS will immediately return on to online operation. If the battery performance indicates a failing battery, the UPS will signal a bad battery via the replace battery LED and/or LCD screen. It will also notify users via PowerChute Business Edition or a Network Management Card if so equipped.

Self Tests can also be manually initiated at any time via PowerChute, The SmartConnect Portal, The Network Management Card, or the front panel of the UPS. If the run self-test button is grayed out in the SmartConnect portal see FAQ FA375690

To manually start a Self Test from the UPS:
  • LCD Screen Models: Go to the "Test & Diags" menu, then select "Self Test"
manual self test via display
  • Legacy Models (No LCD Screen): Press and hold the "I/Test" button. After several seconds the UPS will switch to battery. You can then release the button and the test will continue to completion.
  • self test for old UPS.JPG
Note; Kindly do refer to the User's guide for further details.


SELFTEST FUNCTION:
A new unit with self-test capability will automatically run a self-test on start-up and then run periodic tests on a set schedule, often every 14 days by default. During the test, the UPS will place the load onto battery power to test the strength of the battery.

Schneider Electric Egypt and North East Africa

How does the Smart-UPS Self-Test function work?

Article available in these languages: Spanish, Russian


Issue:

Operation of Smart-UPS Self Test

Product Line:

Smart-UPS, Smart-UPS Online

Environment:

All models, All Serial Numbers

Cause:

All Smart-UPS products feature automatic true load self tests.

Resolution:

By default all Smart-UPS products will perform a Self Test when you initially turn the UPS on, and then once every 2 weeks from that point forward. This can be adjusted via PowerChute, the LCD Screen, or the Network Management Card. The interval will always begin when you last turned the UPS on. There is no way to schedule it to run at a particular time or day.

During a Self-Test the UPS will run on battery for approximately 10 seconds. During this time it will test it's internal subsystems as well as the battery. For a battery test to be valid, it should be charged to 100% before beginning the test.  If an issue is encountered the self test will be aborted and the UPS will immediately return on to online operation. If the battery performance indicates a failing battery, the UPS will signal a bad battery via the replace battery LED and/or LCD screen. It will also notify users via PowerChute Business Edition or a Network Management Card if so equipped. 

Self Tests can also be manually initiated at any time via PowerChute, The SmartConnect Portal, The Network Management Card, or the front panel of the UPS. If the run self-test button is grayed out in the SmartConnect portal see FAQ FA375690

To manually start a Self Test from the UPS:
  • LCD Screen Models: Go to the "Test & Diags" menu, then select "Self Test"
manual self test via display
  • Legacy Models (No LCD Screen): Press and hold the "I/Test" button. After several seconds the UPS will switch to battery. You can then release the button and the test will continue to completion.
  •  self test for old UPS.JPG
Note; Kindly do refer to the User's guide for further details.

 
SELFTEST FUNCTION:
A new unit with self-test capability will automatically run a self-test on start-up and then run periodic tests on a set schedule, often every 14 days by default. During the test, the UPS will place the load onto battery power to test the strength of the battery.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top