Search FAQs
Why am I not able to see my DFB private variables with the OPC UA module BMENUA0100?
Issue:
DFB private variables are not showing with the OPC UA module BMENUA0100
Product Line:
EcoStruxure Control Expert, Unity Pro, M580, OPC UA, BMENUA0100
Resolution:
In order for the OPC UA server to access the DFB private variables, it is necessary to select the option "Include DFB/PU private variables" in the unity project settings under the "PLC embedded data" section
DFB private variables are not showing with the OPC UA module BMENUA0100
Product Line:
EcoStruxure Control Expert, Unity Pro, M580, OPC UA, BMENUA0100
Resolution:
In order for the OPC UA server to access the DFB private variables, it is necessary to select the option "Include DFB/PU private variables" in the unity project settings under the "PLC embedded data" section
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: