{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you migrate DLF 3000 configuration to another computer?
Issue
User is migrating to a new computer and would like to migrate all the DLF 3000 configuration they have done to the new computer.

Product Line
DLF 3000

Environment
Software Migration

Resolution
The configuration files for DLF 3000 are stored in the following file path C:\DLF-3000\Database (note this path is specified when the software is installed and may vary). To transfer the configuration of DLF 3000, all you have to do is copy/replace the two DLFSystem database files over to the new computer in the same file path. Below is a screenshot showing which files need to be copied over to the new computer.


Schneider Electric Egypt and North East Africa