{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Replacement of existing SPD910 Series Differential Pressure Switch ?

Schneider Electric has released an update to the existing SPD910 Series Differential Pressure Switch. Refer to the below table for the replacement of the old model. Process connections and electrical connections remain fully identical. Presets are unchanged and no changes have been made to the existing housing/packaging.
SPD ranges and part numbers
Specification Sheet:
SPD910 Differential Air Pressure Switch Specification Sheet

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: