Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Remote temperature sensor for TC900 series used for?

The RS-03 remote sensor can be used in place of the existing built-in temperature sensor of the TC900 Series thermostats*. It has the same 10 kΩ NTC (3950) element encapsulated in a plastic bulb housing that measures approximately Ø6 x 25 mm and is supplied with 3 m cable (2-wire), finished in all white. The RS-03 sensors are only available in multi-packs of 10 pieces.
*RS-03 works with deluxe models only, i.e. models with an ‘S’ included in the model number (‘DLSA’, ‘DLMSA’, ‘FMSA’, etc.).

RS-03 remote sensor

Schneider Electric Egypt and North East Africa

Explore more
Range:
Category:
Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
Explore more
Range:
Category: