{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
GT block output retained previous true state when condition should have been false
Issue
GT function block output retained a previous true state when the resulting output condition should have been false

Product Line
Control Expert, Unity

Environment
Windows 10, Windows 7

Resolution
GT function block output retained a previous true state when the resulting output condition should have been false

The cause for the issue is due to a detected error condition that occurred during execution or unsuccessful algorithm
execution.  This resulted in the GT function block output retaining a previous state.  The possibility of this issue to occur
when the user logic is configured in a specific function block arrangement is described in the Unity online help and in the
attached resolution.  Recommendations for special consideration when developing the logic to avoid such a situation
is also provided in both the Unity help and resolution.


Examination of the customer application showed that the logic was configured in the function block arrangement that
was recommended to be avoided.

gnd




The following screen capture is from the Unity help:
dbg
gngn

Schneider Electric Egypt and North East Africa

Attachment(s)
EN and ENO description from Unity help..pdf [284.96 KB]
What is the best practice to handle a logic with two Function Blocks in a Jump loop.pdf [1 MB]