{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is maximum number of IEC61850 devices that can be supported by one BMENOP0300 module ?

Dependent on module's mode, the maximum number of IEDs differs :

As Client > max. number of supported IEDs is 32

As Server > max. number of simultaneous client connections is 16 (connection numbers is independent on the number of existing clients. One client could establish more than one connection with the module. Thus, 16 connections do not imply the existence of 16 clients)

For more info, please refer to the attachment

Schneider Electric Egypt and North East Africa

Attachment(s)
BMENOP.pdf [651.63 KB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: