{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is SC3000 relay pack network wiring topology?

SC3000 relay packs can be connected to SER8300 line voltage room controller using one of the following topologies:

  1. Star Topology
  2. Daisy chain Topology
  3. Mixed Daisy Chained & Star Topology
SC3000 relay packs connection topology
NOTE:
  • A maximum of 10 SC3xxxE Relay Packs can be used for a single SER83xxA Room Controller.
  • Only the following models can be Slave Relays: SC3500E5045, SC3400E5045, and SC3300E5045.
  • Only one SC3x4X Relay Pack with monitoring input can be used for a single SERX3xxA Room Controller.

Schneider Electric Egypt and North East Africa