This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
What optional backplates are compatible with my SURT15KRMXLT / SURT20KRMXLT Smart-UPS?
Product Line:
Smart-UPS
Environment:
SURT15KRMXLT / SURT20KRMXLT, All Serial Numbers
Cause:
SURT15KRMXLT / SURT20KRMXLT Smart-UPS feature optional backplates to support different configurations
Resolution:
SURT15KRMXLT / SURT20KRMXLT support the Following backplates:
SYPD3 - (2) L6-20R Outlets, (1) L6-30 Outlet
SYPD7 - (3) L6-20R Outlets
SYPD11 - (2) L6-30R Outlets