This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The TH110 should be associated with a Zigbee concentrator such as ZBRN32,but this one has a Modbus Serial Line Communication .
Accordingly, and as per the attached drawing (Pages from AAM74807 Ind A.pdf) the ZBRN32 can be linked to a PLC. The PLC reads the data of the ZBRN32 (temperature given by TH110) and the PLC could communicate to the Scada by a TCP/IP link by Modbus protocol.
Released for:Schneider Electric Egypt and North East Africa