{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME9.0 - PM8000 vista diagrams not fully translated into Chinese
Product Line
Power Monitoring Expert 9.0

Environment
Vista - Diagrams (Chinese language)

Issue/Cause
Some of the labels are not fully translated to Chinese for the PM8000 default diagrams in Vista.


Resolution
The workaround is to manually change the meter default diagrams (located at C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\diagrams\ud\default) to display the proper language.

Additional Information
This has been fixed in PME 2020.

Schneider Electric Egypt and North East Africa