Product Line
Power Monitoring Expert
Environment
Event Watcher
Resolution
Event Watcher must be configured to use a template the only references Sag/Swell Events.
To create the template follow the steps below:
Configure Event watcher to use the Sag/Swell template by using the following steps.
Power Monitoring Expert
Environment
Event Watcher
Resolution
Event Watcher must be configured to use a template the only references Sag/Swell Events.
To create the template follow the steps below:
- Open Event Watcher by going to Management Console, select Tools >> Reporting Configuration >> Event Watcher Manager
- Select the Templates tab
- Click New
- Give the alarm a name such as PQ Events - Sag/Swell
- If desired, give the alarm a description
- Choose 'Select From Event Log'
- Select Sag/Swell {0.EN_US}|1 Disturbance Start SS1 DistState Disturbance
- Press OK and then apply to save the template
Configure Event watcher to use the Sag/Swell template by using the following steps.
- Inside of Event Watcher choose the Event Watchers tab.
- Select New in the top right
- Give the alarm a name
- Select the Sag/Swell template created above
- If desired, give the alarm a description
- Select the device(s) that the alarm will apply to
- Press OK
Released for:Schneider Electric Egypt and North East Africa