{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to set PID preset references for the ATV630 drive?

Article available in these languages: Spanish

Issue:
Can I program drive to switch between different set points on PID controller for the ATV630 drive?

Product Line:
ATV630

Environment:
All models, all serial numbers

Cause:
Customer wanted to easily switch between three set points, 40, 60 and 80 PSI.

Resolution:
Under the main menu, enter complete setting -> Pump Functions -> PID Controller -> PID Reference -> PID preset references:
Assign a digital input (DI5) for 2 PID Preset Assign
Enter 40PSI for RefPID Preset 2
Assign a digital input (DI6) for 4 PID Preset Assign
Enter 60PSI for RefPID Preset 3
Enter 80PSI for RefPID Preset 4

Note: This function can be accessed if [PID feedback ass.] PIF is assigned.

Schneider Electric Egypt and North East Africa