Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Whether IP address is Mandatory during transferring GOOSE communication between IEC 61850 IED's configuring with Micom relays ?
Description/Issue:
Whether IP address is Mandatory during transferring GOOSE communication between IEC 61850 IED's configuring with Micom relays ?

Product family:
Micom relays

Resolution:
GOOSE is not based on TCP/IP and this will not require an IP address to be configured.
 
Actually Gooses signals are using to send data in an efficient way. Such kind of devices often need to be managed/configured and to do so, other protocols will be used (IEC 61850 MMS, SNMP, DPWF etc..) and such protocols needs an IP address.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: