{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM5110 - Does it comply with IEC 60068-2-6:2007, IEC 60068-2-27:2008?
The IEC60068-2-6 & 2-27 requirements are covered in the PM5110 base standard IEC62052-11.
The Type test report is attached.

Schneider Electric Egypt and North East Africa

Attachment(s)
Type test _ PM5XXX class 0.5S.pdf [1.77 MB]