{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What versions of Vijeo Designer are supported for EcoStruxure Machine Expert?

Article available in these languages: Spanish

Issue
What versions of Vijeo Designer are supported for EcoStruxure Machine Expert v1.0, v1.1 , v1.2.0 and v1.2.2?

Product Line
EcoStruxure Machine Expert, Vijeo Designer

Environment
PLC/ HMI Configuration software on Windows PC

Resolution
See the table below for supported Vijeo Designer versions on EcoStruxure Machine Expert v1.0 and above:
EcoStruxure Machine Expert versionVijeo Designer version that is included with install
v1.0Vijeo Designer is not included
v1.1v6.2.8.1016
v1.2.0v6.2.9.1008
v1.2.2v6.2.9.1008


Notes:
  • EcoStruxure Machine Expert v1.0 was only for PLC configuration and did not include HMI devices in the Logic Builder component. You will need a minimum of EcoStruxure Machine Expert v1.1 to include Vijeo Designer and the HMI devices in the Logic Builder.
  • As of this time of this FAQ's writing (May 2020), there are no additional Vijeo Designer Service Packs published for the above versions.
    However, future Vijeo Designer Service Packs may be found in the Schneider Electric Software Update Tool launched from the Windows Start -> Programs -> Schneider Electric -> Software Update -> Software Update (shortcut icon)"
  • It is recommended that only one version of EcoStruxure Machine Expert (or SoMachine) be installed on one Windows PC at a time.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: