Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Is the EcoStruxure OPC UA Server Expert compatible with Windows 7 Embedded?
Issue
Windows 7 Embedded is used in the most part of the Industrial PC and customers want to know if this version of Windows is compatible with EcoStruxure OPC UA Server Expert.

Product Line
EcoStruxure OPC UA Server Expert, Harmony iPC

Environment
EcoStruxure OPC UA Server Expert v2.0, Windows 7 Embedded

Resolution
The Windows 7 Embedded  (WES7) version is built on the same framework than Windows 7 Ultimate. So, any software compatible with a standard Windows 7 distribution will also run properly on WES7 that has been develop for critical infrastructure like ATMs, Medical Equipment and PC that controls machines on a factory. These applications does not need extra features, they need long term stability and few updates that is the proposed of the WES7 including the resource to choose the features you need in your OS.

So, a PC with Windows Embedded is compatible with EcoStruxure OPC UA Server Expert if it follows the standard requirements of the software described below:
Host PC Software Requirements

EcoStruxure™ OPC UA Server Expert can be installed on a host PC running Microsoft Windows™ 7, Windows 10, Windows Server 2012 R2, and Windows Server 2016 platforms.

NOTE:

For Windows 7 platforms, you may need to separately install Microsoft .Net Framework 4.5.
For Windows Server 2012 R2 and Windows Server 2016 platforms, remote desktop services are not supported.
EcoStruxure™ OPC UA Server Expert can run on the above-referenced platforms in a virtual environment. Note that server performance in a virtual environment setting may be negatively impacted by high activity demands on the host resources, and by Ethernet adapter emulation (in a NAT system).

Host PC Hardware Requirements

EcoStruxure™ OPC UA Server Expert runs on a PC that meets the following minimum standards:

either a 32-bit or a 64-bit platform
Minimum RAM of 4 Gb (recommended 16GB)
Multicore \ multiprocessor architectures are recommended, to enable optimal runtime performance.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: