{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will VJD Runtime connect to the backup IP in Modbus TCPIP driver if the PLC is in stop status
  1. Issue
After select the secondary connection in Modbus TCPIP Driver, will VJD runtime switch to the backup IP if the PLC is in stop status

  1. Environment
Vijeo Designer 6.2.
  1. Resolution
Only a communication failure is detected on the primary IP, then VJD runtime will switch to the backup IP. If the PLC is in stop status but the communication is still active, then runtime will not switch to the backup IP.

User can consider to change the Equipment's IP address in script if the PLC in detect is in stop status.
Here is an example to change the Modus TCP Equipment's IP:

int[] ipAddress = {192, 168, 1, 10};

ModbusEquipment01.openConfig();

ModbusEquipment01.setProperty("Con_IPAddress", ipAddress);

ModbusEquipment01.commitConfig();
  1. FAQ Applicable Conditions
FAQ applies to all Vijeo Designer 6.2 SPx.

Schneider Electric Egypt and North East Africa