{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I preprogram IP address of the Profinet Communication Module (VW3A3627) for the ATV320 and install into another ATV320?
Issue:
Is the IP address retained in the VW3A3627 for the ATV320 drive?

Product Line:
Altivar ATV320

Environment:
All serial numbers, all model numbers

Cause:
Customer want to have a preprogram IP address on Profinet Communication module (VW3A3627) so he didn't have to program when installed into the drive.

Resolution:
No, you cannot preprogram the IP address for the Profinet Communication Module (VW3A3627) because the address is not retained in the Card.


Schneider Electric Egypt and North East Africa