{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Will data sharing between SmartX IP controller devices stop when the hosting EBO server goes offline?
Issue:
If the communication is lost between SmartX controller devices and hosting EBO server, will the data sharing between SmartX controller devices continue to work?

Product Line:
EcoStruxure Building Operation, SmartX controller devices

Resolution:

External bindings is the recommended way to share data between SmartX IP controller devices (MP-C, MP-V, IP-IO, RP-C) or between SmartX IP controller devices and 3rd party BACnet devices.  External bindings help facilitate direct peer to peer communication in such environments. For example, if SmartX IP controller1 requires a temperature value from SmartX IP controller2, it can utilize an external binding to directly exchange that temperature value without communicating through the server. In addition, in those networks where an EcoStruxure BMS server is present, you can utilize an external binding to lighten the burden of inter-SmartX IP controller traffic on that server.

Machine generated alternative text:EBO Server Analog Value Analog Value MPX controller cons am Value Pont MPX controller cons am Prograni Value Point Third Party A Analog Value Third Party B Analog Value
If the external binding is used for data sharing, the data sharing between SmartX IP controller device will continue even if the SmartX server (Automation Server or Enterprise Server) is offline. If the standard server binding is used, data sharing will stop if the SmartX server goes offline, as data shall flow though the SmartX server.

For more information, refer to below WebHelp articles:
https://ecostruxure-building-help.se.com/bms/Topics/show.castle?id=12365
https://ecostruxure-building-help.se.com/bms/topics/show.castle?id=11699

Schneider Electric Egypt and North East Africa