{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What can cause AC drive input fuses to blow-up?
The blown fuse is a symptom of the true problem.
A fault of some type has caused the fuse to blow, and this could be for several reasons as:
  • Quick repetitive switching to mains by applying input power more quickly causes the inrush limiters to overheat in the input precharge circuit and eventually burns them out. The dc bus capacitors don’t have enough time to discharge. If the input circuit doesn’t have time to stabilize, additional input current can blow the input fuses or circuit breaker and damage the charge circuit.
  • Poor Earthing system and not following the EMC installation guidelines.
  • Capacitor bank may result in undesirable resonant currents.
  • Transient perturbation associated with the supply switching.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.