{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to do a factory reset using SoMove for the Altivar Process Drives?
Issue:
Can I do a factory reset on the Altivar Process drive using SoMove Software?

Product Line:
ATV630 ATV930

Environment:
All serial numbers, all model numbers

Cause:
Customer had SoMove connection to the drive, and he wanted to use SoMove for factory reset.

Resolution:
Go to the Device tab on top of SoMove, select Factory Setting then choose Customize or Execute.
d

For Customize: select OEM or Schneider Electric factory settings and click OK.  (Use OEM if directed by the equipment supplier).
d

For Execute: select All parameters or other options such as Drive configuration, Motor Control, Communications, Display Configurations and click apply.
Screenshot 2022-09-26 141515.png
You will have to acknowledge the Warning making sure you understand the risk before the Factory reset will be performed.
Screenshot 2022-09-26 141822.png
When the reset is complete you should see this dialog box:
d

Schneider Electric Egypt and North East Africa