Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the maximum reading of kWh on the EasyLogic PM2100 display?
Issue:
In the product data sheet, digits maximum display digits is 12, but the meter resets at 1 GWh.

Environment:
EasyLogic™ PM2100

Resolution:
The maximum reading on the meter display is 12 digits. However, the last 3 digits are fractional values. So the maximum kWh reading for the meter display is 999999999.999 kWh.

Example:
The following describes a kWh reading of 348721569.857:

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: