Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can a PM2000 or PM5000 series meter operate above 2000m?
Issue:
Its not mentioned whether these power meters can operate at altitued higher than 2000m.

Environment:
EasyLogicâ„¢ PM2000 series
PowerLogicâ„¢ PM5000 series

Resolution:
We are not recommending either of these devices to use above it's specified altitude. During our testing, we have noticed some issues with creepage and clearance requirements when it is used above 2000m altitude.

Schneider Electric Egypt and North East Africa