Issue:
Can access "Test Mode Screens" via the front panel, regardless of actual user permissions configured.
Menu->Normal Display Mode->Test Mode
Product:
PM8000 and ION7400 on both integrated and remote displays.
ION9000
Resolution:
No actions require, the meter will remain in normal mode. The mode shows "NORM" in the display header, and the output register of the Test Mode Enable external boolean module remains "False".
Released for:Schneider Electric Egypt and North East Africa