Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Could not write to Event log pipeline in Alarm Service." after upgrading PME

Issue
Events from devices and Software Alarms don't show up in Alarms and are not written to the database.


Example of the error message in the  System Log:
 

ID: 3367495

Timestamp: 13/02/2020 9:40:38,107

Priority: ERROR

Source: Software Data Processing Service

Target: EventLogWriter

Category: Computer General

Computer: EU01SDP078

Description: Could not write to Event log pipeline in Alarm Service.

 

 

ID: 3367494

Timestamp: 13/02/2020 9:40:38,087

Priority: ERROR

Source: Software Data Processing Service

Target: LogAcquisitionMessenger

Category: Computer General

Computer: EU01SDP078

Description: Message Write Failure: Error sending message on queue '.\private$\LogSubsystemPrimaryRouter_Data'.; ErrorCode: [AccessDenied]; Body: DataMessage: Operation [Insert]; Filtered [False] Retry [0]



Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
PME Web Application

Alarms



Cause
The ION Log Subsystem Router Service is running under a user that does not have access to the message queues or the message queues were not built correctly.

Resolution
Confirm that the user permissions for the Log Subsystem Router Service is allowed access cloudagent_control, cloudagent_data, logsubsystemprimaryrouter_control, logsubsystemprimaryrouter_data, logsubsystemsecondaryrouter_control, logsubsystemsecondaryrouter_data Private Queues. 

  1. Open Computer Management on the PME Server.
  2. Open Services and Applications > Message Queuing > Private Queues

example of message queues

  1. Right click on each of the 6 queues, select Properties, and open the Security tab.
  2. Confirm each of these queues permissions:
    1. "Everyone" group has access to allow:
      • Get Properties
      • Get Permissions
      • Send Message
    2. "Administrators" group should have full access to the queue
    3. "ANONYMOUS LOGON" group should only have access to:
      • Send Message

If adding everyone does not solve the issue then recreate the queues:

  1. Stop all PME services
  2. Delete the 6 message queues
  3. Start the Network Router Service
  4. Start Log Inserter Service
  5. Start the Log Subsystem Router Service
  6. Start all other PME services

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: