This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
Need to know the function of SmartX IP controller devices USB ports
Product Line:
EcoStruxture Building Operation, SmartX IP controller devices
Resolution:
1. MP Series controllers, and IP-IO modules:
MP Seriescontrollers, MP-C, MP-V, and IP-IO modules, have two USB ports, host and device ports. These ports are reserved for future use
.
2. RP Series controllers:
RP Series controllers have two USB ports, host and device port.
The USB host port is a USB 2.0 type-A port, which is rated 2.5 W. The USB host port can be used for connection of the Smart Zigbee Adapter to add Zigbee TM wireless connectivity to the RP-C controller, requires EBO V3.2 or higher and RP-C firmware V3.0.2.01 or higher. The Smart Zigbee Adapter can be used to extend the controller's point count and bring flexibility in retrofit applications.
Need to know the function of SmartX IP controller devices USB ports
Product Line:
EcoStruxture Building Operation, SmartX IP controller devices
Resolution:
1. MP Series controllers, and IP-IO modules:
MP Seriescontrollers, MP-C, MP-V, and IP-IO modules, have two USB ports, host and device ports. These ports are reserved for future use
.
2. RP Series controllers:
RP Series controllers have two USB ports, host and device port.
The USB host port is a USB 2.0 type-A port, which is rated 2.5 W. The USB host port can be used for connection of the Smart Zigbee Adapter to add Zigbee TM wireless connectivity to the RP-C controller, requires EBO V3.2 or higher and RP-C firmware V3.0.2.01 or higher. The Smart Zigbee Adapter can be used to extend the controller's point count and bring flexibility in retrofit applications.
The USB device port is a USB 2.0 mini-B port. The USB device port is reserved for future use.
Released for: Schneider Electric Egypt and North East Africa