This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
Fan connected to SE8350 room controller stays running at low speed when there is no demand
Product Line:
SE83500 room controllers
Resolution:
There are three possible causes:
Fan connected to SE8350 room controller stays running at low speed when there is no demand
Product Line:
SE83500 room controllers
Resolution:
There are three possible causes:
- The “Fan mode” is set to “Low” instead of “Auto”.
- Auto selection will activate fan on demand.
- The “Auto Fan func.” is set to “AS”.
- Change the setting to “AS / AD”.
- AS: In Occupied, Standby, and Override modes, the Fan stays ON at low speed even if there is no demand for Heating or Cooling. In Unoccupied mode, the Fan turns Off when there is no demand for Heating or Cooling.
- AS/AD: In any Occupancy mode, the Fan turns Off all speeds when there is no demand for Heating or Cooling.
- The Dehumidification is activated.
- If dehumidification is not required, set the “Deh. lockout” parameter to “Disable”.
Released for:Schneider Electric Egypt and North East Africa