Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Default IEC 61850 port number in ION meters
Issue
What is the default IEC 61850 port number in ION meters?

Product Line
ION8650, ION7650

Environment
IEC 61850 protocol over Ethernet

Cause
The meter can be integrated into an IEC 61850 system as an IED (or server), supporting concurrent IEC 61850 client connections.

Resolution
Default port number is 102 and can be changed if necessary. The settings are in Ethernet Communication module:

IEC 61850 where to change port number in ION Setup Ethernet Communications Module

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: