This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue:
Need to configure EBO IoT interface to publish data to Azure IoT Hub via MQTT protocol.
Product Line:
EcoStruxure Building Operation
Resolution:
MQTT is a lightweight and flexible data transfer protocol for IoT resources. EcoStruxure Building Operation, V3.2 or higher, can be configured to send data to an MQTT broker on interval or event-driven. The below are the tested brokers:
Refer to EBO WebHelp for more information:
https://ecostruxure-building-help.se.com/bms/Topics/show.castle?id=13597
Need to configure EBO IoT interface to publish data to Azure IoT Hub via MQTT protocol.
Product Line:
EcoStruxure Building Operation
Resolution:
MQTT is a lightweight and flexible data transfer protocol for IoT resources. EcoStruxure Building Operation, V3.2 or higher, can be configured to send data to an MQTT broker on interval or event-driven. The below are the tested brokers:
- Microsoft Azure IoT Hub
- Amazon IoT Core
- IBM Watson IoT
- Mosquitto
Refer to EBO WebHelp for more information:
https://ecostruxure-building-help.se.com/bms/Topics/show.castle?id=13597