Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How to connect 3-wire sensor by using BMXDDI3202 and BMXDDI6402?
  1. Issue

The wiring diagram in the manual only shows the 2-wire sensor connection of the module. Is there a wiring diagram for 3-wire sensor when using BMXDDI3202 and BMXDDI6402?

  1. Product Line
X80 IO module
  1. Environment
BMXDDI3202, BMXDDI6402
  1. Resolution
Please check the below picture which is a wiring diagram example for 3-wire sensor connection only for reference.

Comparing to the 2-wire sensor connection, customer need to add a Fuse in the single loop which the capacity should follow the off-status current in the sensor manual.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: