{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What’s the equivalent function of clear events in IEC101/IEC104?
  1. Issue
As for the BMXNOR0200 platform, what’s the equivalent function of clear events in IEC101/IEC104?
  1. Environment
BMXNOR0200, IEC101/IEC104
  1. Resolution

We have the equivalent command in the IEC101/IEC104 protocol.
It is C_RP with QRP=2: reset of pending information with time tag of the event bugger.
[NOR has no interface]





Schneider Electric Egypt and North East Africa