{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to migrate a Safety application for Modicon M580 / EcoStrucxure Control Expert with a Safe Peer to Peer communication from ECE<15.0 to ECE>=15.0 and a CPU FW >= 3.20
Issue
  • Modicon M580 Safety with EcoStrucxure Control Expert V15 implements a new safety time management principle no more based on NTP services.
  • New peer to peer communication EFB are provided to replace legacy ones.
  • Compiling an earlier application containing legacy EFBs will lead to compilation errors.

Environment
  • ECE>=15.0 and CPU FW >= 3.20

Resolution
here is the list of steps to go through :
  • Set the application level to 3.20
  • Suppress in the logic each instance of S_SYST_CLOCK_MX
  • Replace in the logic each instance of the S_RD_ETH_MX FB with the S_RD_ETH_MX2 FB.
  • Replace in the logic each instance of the S_WR_ETH_MX FB with the S_WR_ETH_MX2 FB.
  • Create and connect the CONTROL_DATA to each of the S_RD_ ETH_MX2 / S_WR_ ETH_MX2 FB
  • Add the communication transfer of the CONTROL_DATA from Receiver PAC to Sender PAC
  • Do you want to delete all unused SAFE variables?
    • yes
      • Purge all unused variables in the Safety Data Editor, in the Function Blocks folder
      • Purge unused Type in the Derived FB Types Editor
    • no
      • Delete manually all S_RD_ETH_MX & S_WR_ETH_MX variables, in the Function Blocks folder
      • Delete manually all S_RD_ETH_MX & S_WR_ETH_MX FB types, in the Derived FB Types Editor
  • Purge unused Types in the Types Library Manager  – in the <Application> view of the types

FAQ Applicable Conditions (Optional)
Both CPU linked via peer to peer must be version SV3.20 or later

Schneider Electric Egypt and North East Africa

Attachment(s)
S_RD_ETH_MX2_FB.PNG.png [180.12 KB]
S_WR_ETH_MX2_FB.PNG.png [108.72 KB]
Purge unused Types in the Types Library Manager in the Application view of the types.PNG.png [89.64 KB]
purge safety data editor.PNG.png [97.64 KB]
Purge unused Type in the Derived FB Types Editor.PNG.png [202.8 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.