Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Modbus register list for SLP series Temperature sensors and Humidity sensors
Issue:
Need Modbus register list from SLP series Temperature sensors and Humidity sensors
Environment:
SpaceLogic Room Units
Resolution:
The SpaceLogic SLP Series of air quality sensors for living space is a flexible multisensor platform for use with BAS controllers designed to accept BACnet or Modbus outputs.
Function Code:
Note that an attempt to write to “read only” holding registers will give an error and the entire write command will not be executed even if writing to read/write locations were also requested. Exception code 2 is given in this case. “Preserved” means the values is maintained through power outages.
![Input Register](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009FnzTQAS&oid=00DA0000000abSm)
![Holding Registers](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009FnzZQAS&oid=00DA0000000abSm)
Need Modbus register list from SLP series Temperature sensors and Humidity sensors
Environment:
SpaceLogic Room Units
Resolution:
The SpaceLogic SLP Series of air quality sensors for living space is a flexible multisensor platform for use with BAS controllers designed to accept BACnet or Modbus outputs.
Function Code:
Note that an attempt to write to “read only” holding registers will give an error and the entire write command will not be executed even if writing to read/write locations were also requested. Exception code 2 is given in this case. “Preserved” means the values is maintained through power outages.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Category:
Range:
Explore more
Category:
Range: