{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ConneXium DRS Predefined Switch configuration profiles C17 and C18
Issue
ConneXium DRS (Dual Ring Switch) configuration C17 and C18 are new predefined configuration profile for Ethernet RIO, made available in September 2020.

Configuration Filenames:
C17_Master_RIOMainRingFx_RIOSubRingTx_DIOCloudsV1.4.cfg
C18_Slave_RIOMainRingFx_RIOSubRingTx_DIOCloudsV1.4.cfg

Although similar to the C11 and C12 DRS predefined configuration profiles, the C17 and C18 configuration profiles use Fiber port# 1 for the Main Ring and Fiber port# 2 for the first of two redundant ring connections between the two switches. Port# 5 copper wire connection is still used to connect all the drops of the sub-ring between the two switches as before. But port# 6 copper wire connection goes to two NRP module located at the first two drops as the second redundant ring connection between the two switches to span the extended distance. All other ports remain the same.

Image1


Product Line
The C17 and C18 predefined profiles are used with Connexium Extended Dual Ring switches:
TCSESM063F2CU1 ConneXium extended dual ring switch that has 2 ports that support multimode fiber.
TCSESM063F2CS1 ConneXium extended dual ring switch that has 2 ports that support singlemode fiber.


Resolution
Profiles C17 & C18 are found in the file, "Predefined DRS Configuration files v1.4 for use with Ethernet Remote IO.7z"

Install configuration files:
C17_Master_RIOMainRingFx_RIOSubRingTx_DIOCloudsV1.4.cfg
C18_Slave_RIOMainRingFx_RIOSubRingTx_DIOCloudsV1.4.cfg

Schneider Electric Egypt and North East Africa