Is the "modular contactor" is only applicable for the 'LED lighting' application in Ecodial ?
No, The 'MODULAR CONTACTORS can be used for the smooth operation of any lighting application. The different lighting applications are already available in Ecodial.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
EcoStruxure™ Building Operation
EcoStruxure Building Expert
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.