{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the cable sleeve for a XAC pendant station replaceable part?
Issue:
What is the part number for a replacement cable sleeve for a XAC pendant station?

Product Line:
Push Buttons and Operator Interface

Environment:
22mm XAC Pendant Station Control


Answer:
XACA960 is the part number for replacement cable sleeve for general purpose units (Empty station references XACA0**)
XACA02, XACA03, XACA04, XACA05, XACA06, XACA08, XACA12

XACB960 is the part number for the
replacement cable sleeve for general purpose units (Empty station references XACB0**)
XACB02, XACB03, XACB04, XACB05, XACB06, XACB08, XACB12

XACA913 is part number for replacement cable sleeve for small hoist pistol grip style
XACA201(4), XACA205(4), XACA211(4), XACA215(4), XACA207(4), XACA217(4)

XACD901 is the part number for replacement cable sleeve for the XACD series stations.

Schneider Electric Egypt and North East Africa