{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the replacement coil for the electrically held 8903L lighting contactor?

Issue:
Replacement coils for 8903 Type L contactor:

Product Line:
8903 type L Lighting contactors

Environment:
North American Product

Cause:
Maintenance

Resolution:
This depends on pole quantity and voltage:
2-6 poles, 9998L**
7-12 poles, 9998LH**
PolesCoil Class and Type HZSuffix Number
(complete coil number consists of the class and type followed by the suffix)
Coil VA
24v 110-115v 120v 208v 220v 240v 277v 380v 440v 480v 550v 600v Inrush Sealed
2-69998L 6023-4450[*]5355--62-6515030
50244445525354-606263656614030
8-12 9998LH6023-4450[*]5355--62-6518035
50244445-5354-6062-65-17035

* - use a 60 Hz coil of the next higher voltage

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: