{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are the 9001 KA contact blocks gold flashed?

Issue:
Do we have contact blocks with gold flashed terminals for 30mm push buttons?

Product Line:
Push Buttons and Operator Interface

Environment:
30 mm Push buttons and accessories

Resolution:
Not on the standard contact blocks. We have a 9001KA3* series that has gold flashed contacts.

1NO and 1NC - 9001KA31
1NO - 9001KA32 (OBSOLETE)
1NC - 9001KA33
1NO Early Closing - 9001KA34
1NO Late Opening - 9001KA35

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: