{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is the Vijeo Designer project file .vdz included in the file system download files ?

Issue:
Vijeo Designer project file .vdz included in the file system download files


Product Line:
Vijeo Designer


Resolution:
The only way the vdz file would be included in the File system download files, is if the "include editor project" option was enabled in the project. If this is the case, the vdz file is located in the following path PUBLIC\PROJECTS\TARGET1\DATA\PROJECT. TARGET1 folder is the default name for the target, this could be a different name. If the vdz file is not located in this path, then the "include editor project" option was enabled in the project and therefore the vdz file would not be included.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: