How Copro ETY of Primium could be converted to BMENOC03x1 or M580 CPU
If the I/O scanner’s R/W size of ETY Copro of premium CPU is not less than 1KWords , this I/O scanner will be converted to BMENOC03x1, while IOSCANNING of ETY port will be converted to M580 CPU if I/O scanner’s R/W size is less than 1Kwords
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.