{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why Firmware Upgrade of my Smartlink Modbus Fails ?

Product Line
Smartlink Modbus A9XMSB11

Environment
A9XMSB11 + EcoStruxure Power Commission

Issue
Smartlink Modbus firmware upgrade failed each time with EcoStruxure Power Commission.

Cause of Issue
There is a known gap when you upgrade the FW with a Serial Link speed of 9600 Bauds.

Prevention
Ensure that your serial link speed is higher than 9600 Bds.

Resolution
To change the Serial Link speed of your Smartlink, you need to perform a Factory Reset.
To reset the Acti 9 Smartlink factory settings (pulse weight at value 10, meters at 0, communication
parameters), proceed as follows:

  1. De-energize Acti 9 Smartlink
  2. Set the Modbus address to value 00
  3. Re-energize Acti 9 Smartlink
  4. Set the selected address

Automatic adaptation to the communication parameters only occurs on powering up the Acti 9 Smartlink. After receiving a maximum of 25 frames from the master, Acti 9 Smartlink automatically adapts its communication parameters to those of the master (speed, parity and number of stop bits).

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: