{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
PX250 / 500 MIM or RIM Not Communicating to NMC
Issue:
After FW upgrade or replacement of the Intelligence Modules, the Network Management Card (NMC) stops communicating with them.  When logging in through the web interface, the NMC shows “Device Initializing”.  Firmware is correct, and in some cases, upgrading or downgrading the firmware fixes the issue. 

Example:
MIM is replaced.  The FW is upgraded to 4.37, and everything is working fine.  Logging into the NMC shows “Device Initializing” but communication is never restored.

Product line:
Symmetra PX 250 / 500, AP9635

Environment:
All models, all serial numbers

Cause:
Security Settings have been changed to comply with the California Laws.  Sometimes during firmware upgrade, downgrade, or Intelligence Module replacement, the Smart Slot Settings change from “read/write” to “No Access” which causes the NMC to lose communication with the IMs.

Resolution:
Go to the smart slot setting from the display and change it back to “read / write”.  If necessary, reboot the NMC card.  Communication will be re-established with the IMs.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.