Search FAQs
Adding an Ethernet module (BMXNOC040x, 140NOC78xxx ) causes Control Expert 15 to close.
Adding a BMXNOC040x or 140NOC78xxx to the applicable rack will return the following error message. This will be followed by an unexpected closure of Control Expert 15.
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009wLOMQA2&oid=00DA0000000abSmMAI)
This issue will occur if the module is added to a Control Expert application after installing the following hot fixes
This issue applies to the following DTM related modules::
M580 :
M340 :
Quantum :
The following steps can be used as a workaround,
This issue will be fixed in a soon to be released hot fix.
This issue will occur if the module is added to a Control Expert application after installing the following hot fixes
- 'ControlExpert_V150_HF0380584E'
- ControlExpert_V150_HF_Integrity_Check'
This issue applies to the following DTM related modules::
M580 :
- BMXNOC0402
M340 :
- BMXNOC0401
- BMXNOC0401.2
Quantum :
- 140NOC78100,
- 140NOC78100.2,
- 140NOC78000,
- 140NOC78000.2
The following steps can be used as a workaround,
- Uninstall Control Expert.
- Reinstall Control Expert.
- Install all hot fixes except 'ControlExpert_V150_HF0380584E'.
This issue will be fixed in a soon to be released hot fix.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: