{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an ATV12 be powered on with 460V AC power?
Issue:
Is it possible to connect 460Vac input power supply on the ATV12?

Product Line:
ATV12

Environment:
All model numbers, all serial numbers

Cause:
Customer only has 460V input power supply.

Resolution:
No, it is not possible to power on the drive with 460Vac power supply.  Two standard versions of ATV12 are available:

Drive voltages

Schneider Electric Egypt and North East Africa