{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the ConneXium DRS Predefined Switch configuration profiles C19 and C20?
ConneXium DRS (Dual Ring Switch) configuration C19 and C20 are new predefined configuration profiles for Ethernet RIO, made available in June of 2021.

The two Configuration Files are:
1.  C19_Master_RIOMainRingTx_RIOSubRingFxTx_DIOCloudsV1.5.cfg
2.  C20_Slave_RIOMainRingTx_RIOSubRingFxTx_DIOCloudsV1.5.cfg

Although similar to the C11 and C12 DRS predefined configuration profiles, the C19 and C20 configuration profiles use copper port#5 from both switches for the Main Ring Outer connection and port#6 between both switches for Main Ring redundant Inner connection. Fiber Port#1 of both switches are used for the Sub Ring Outer connection and port#3 between both switches are used for the Sub Ring redundant Inner connection.  NRP modules are used to connect between fiber and copper of the CRA module at the drop.  All other ports for DIO Cloud connections remain the same.

The C19 and C20 predefined profiles are used with Connexium Extended Dual Ring switches:
TCSESM063F2CU1 ConneXium extended dual ring switch that has 2 ports that support multimode fiber.
TCSESM063F2CS1 ConneXium extended dual ring switch that has 2 ports that support singlemode fiber

Profiles C19 & C20 are found in the file, "Predefined DRS Configuration files v1.5 for use with Ethernet Remote IO.7z"

C18 and C19 example diagram

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: